5/22/2024 4:33 PM | |
Posts: 5 Rating: (0) |
Hi, I am having a similar problem where I can upload the program over ethernet, but when I try to do it with a microSD card, the LOGO! says the card is empty. It is a new, 32 GB card, formatted to be FAT32. I have followed the User Manual section 9. Saved the program using the Save As > .bin function in LSC. The LOGO_U_P.bin file is the only one on the card. Is there some particular formatting other than default for the SD card? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2024 04:15:38New subject after splitting Last edited by: Jen_Moderator at: 05/23/2024 04:16:27Spelling mistake corrected. |
|
Follow us on