9/19/2015 4:11 AM | |
Posts: 2 Rating:
|
Good day everyone! May I please seek your assistance and expert advise on how to address my problem with our project. The set-up is as follows: We have an existing PLC System (See attached) which is working fine. Now, we need to add an Analog input module to get ampere readings from 8 sets conveyor drives (Will add more in the future). We use an ET200M Remote I/O Interface module and physically connect the 8-channel analog input module (6ES7331-7anKF02-0AB0). Then link the additional system to the existing PLC system via a SCALANCE X206-1LD Industrial Ethernet Switch. My question is how can I read data from the analog input module in this setup? Any comments, advise and assistance will be greatly apreciated. Thank you and regards, Gado AttachmentCrusher PLC Hardware Arrangement_Modified.docx (103 Downloads) |
Follow us on