Industry Online Support
Technical Forum
9/19/2012 12:41 PM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
Cant see PLC (s7-1200) in WinCC RT simulation (where are NOT connect) ?! Is it internal (programming) or external (windows,Firewall) problem? I can see PLS in Step7 (can download and online monitoring), but CAN NOT see when start RT Simulation I use wireless connection (wi-fi), Step7 prof., WinCC prof. HMI connection - OK PG/PC Interfac Test - OK Firewall and anty-virus - Turn OFF Tks
Attachmentwincc.zip (753 Downloads) |
Follow us on