2/20/2017 7:17 AM | |
Posts: 21 Rating:
|
Hello, I am using CB 1241 for modbus communication with DSP. DSP supports the RS 485 communication. I programmed the port with Slave address -1 , baud rate - 9600, parity - none. I am using TIA V13 software, and programmed the with MB_COMM_LOAD and MB_MASTER with version 2.1 I set the same slave address, baud rate and parity as mentioned in the DSP. MB_COMM_LOAD is working fine. (DONE is TRUE) but for MB_MASTER i am getting BUSY signal is TRUE as long as REQ is HIGH, and BUSY is FALSE as long as REQ is LOW. I am not getting any ERROR signal. I have tried changing the terminals of the terminals Rx and Tx, but still no result. I don't know why i am getting BUSY signal. please help me to solve the problem. With Regards, PCNS ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/20/2017 3:22:29 PMNew subject after splitting |
|
2/22/2017 7:42 AM | |
Posts: 21 Rating:
|
Hello, AttachmentNew folder.zip (248 Downloads) |
Follow us on