11/22/2017 7:29 AM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating: (4) |
Hello Tungpt3149, I have grouped the AS blocks as described in the following entry, https://support.industry.siemens.com/cs/ww/en/view/28757820 I have successfully configured the blocks and faceplates, but the issue is that i am not able to operate the block. it hold the last command and do not accept the new command afterwards. Actually with the "Manual" selection from the faceplate the block IO "ManModOp" changed from "0" to "1" and this value hold there continuously. so it does not accept the "Automatic" command from the faceplate. Please suggest the solution for the issue. Best regards, nkr |
Last edited by: nkr at: 11/22/2017 7:38:28 AM |
|
Follow us on