5/24/2023 7:25 AM | |
Joined: 4/10/2006 Last visit: 4/14/2025 Posts: 959 Rating:
|
Hi ChristophD, in the attachment I have visualized what the project will look like... I can have a certain number of operator panels of the same type but all with different screens and layouts. When I need to connect one to the PLC (I only have one cpu) I have to be able to do it with a number in a word, attributing a number to a connection example: if I write 1 in a variable, I connect the PLC with the HMI connection PLC01 if the variable is 2, I connect the PLC with the HMI connection PLC02 if it is 3, I connect the PLC with the HMI connection PLC03 ............... if it is 22, I connect the PLC with the HMI link PLC22 in this case I can't use the "ChangeConnection" instruction in any way because it doesn't show me any connection. Maybe they should all be together like in my first post. But so far it doesn't matter. In such a configuration where I have many HMIs but can only connect one at a time, how do I do this? It's possible? Thank you Attachmenthmi.pdf (301 Downloads) |
Setting of my PG M6 Siemens |
|
Follow us on