3/11/2015 10:26 PM | |
Joined: 8/18/2010 Last visit: 3/18/2023 Posts: 42 Rating: (9) |
Anyone else having issues assigning a configured connection to the connection property of the Change Connection function? When I add Change Connection to an event and try to pick my connection, the only selection available is Internal Tag. TP900 Comfort S7-1214 DC/DC/DC V4.0 TIA Portal V13 SP1 Upd1 Wincc Adv Step7 Pro AttachmentScreenShot.pdf (183 Downloads) |
Follow us on