6/2/2011 9:27 AM | |
Posts: 34 Rating: (0) |
Hi everyone, I want to change the picture of a standard Block icon in @PCS7Typicals.pdl.. How can it be done? Please help me. Thanks & Regards. Chetna |
6/2/2011 9:54 AM | |
Posts: 691 Rating: (37) |
You can edit the Block Icons. Open @PCS7Typicals.pdl , select the desired Bolock Icon and right click. Choose Coustomized Objects-> Edit, in that you will see an object Status Display showing some pic. You can modify that with the help of its properties. Once you finished editing, select all the Block Icons object , then right click -> Customized Objects -> Finish Editing. Once you do OS Project Editor all the Block Icons resets to by default Configuration How can you create your own block icons that will be incorporated |
6/2/2011 1:59 PM | |
Posts: 691 Rating: (37) |
Dear Chetna The pic you have given is already in Edit mode. The reason that is Dark Black is that it has been used by the Block Icon Property. Please refer to the above posted link for Creating Block Icons. First you close this Pdl without saving anything and then re-open it and then go for edit |
6/2/2011 2:14 PM | |
Posts: 34 Rating: (0) |
Hi, I have done exactly the same way as the procedure is but 'configuration dailog' is not coming active. take a look at the attchment. Thanks. Chetna |
Follow us on