5/26/2014 11:18 AM | |
Posts: 784 Rating:
|
Hello, If we wantto change the setting of HW,we connect online into CPU via TIA Portal. Best regards...... |
5/26/2014 11:44 AM | |
Joined: 3/21/2006 Last visit: 12/18/2022 Posts: 10221 Rating:
|
The output ranges (SM1232) are voltage (+/-10V)or current (0-20mA only).If you want to write 4-20mA is another story...http://support.automation.siemens.com/WW/view/en/42087579 |
Last edited by: UMENCHO at: 5/26/2014 11:46 AM |
|
This contribution was helpful to
2 thankful Users |
5/26/2014 5:10 PM | |
Posts: 559 Rating:
|
It is not possible. The range & typeof signal of analog module is defined in hardware configuration of CPU. So it is not possible to change from OP. |
5/27/2014 9:18 AM | |
Posts: 4 Rating:
|
Hello, |
Follow us on