5/30/2008 10:46 AM | |
Posts: 5822 Rating: (412)
|
Hello, I just wonder, do you use the AG_RECV V 4.7 in your PLC? Because with this Block some issues have been solved, on of it was the issue with the 80B1 Status... that occurred occasionally. Please load the latest SIMATIC NET Library at: SIMATIC_NET_CP Library in STEP7 / NCM S7 bis V5.4 SP3 and PROFINET Library for iMAP V2.0.1 There the function have been fixed. Best regards J_Bell |
5/30/2008 1:27 PM | |
Posts: 5822 Rating: (412)
|
Hello, the AG_SEND is no problem, but the Version 4.6 of the AG_RECEIVE is. Please exchange the FC with the Version 4.7. Best regards J_Bell |
Follow us on