1/12/2016 10:38 AM | ||||||||||
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, New Characteristics for Motor Protection with 8-Channel Analog Input Module 6ES7 331-1
New IM153-2 with New Functions Released for Delivery
you can change both modules without changing any software. regards, |
|||||||||
FCK WAR! |
||||||||||
1/12/2016 10:43 AM | |
Joined: 5/12/2006 Last visit: 11/29/2023 Posts: 21947 Rating:
|
Hello, you get such information in the produktdetails page: AO-Card : https://support.industry.siemens.com/cs/de/en/view/39980695 Spare part replacement: The new module will replace the module below and is spare part compatible. This means that a module with order no. -1KF01- can simply be replaced by the new module with order no. -1KF02- without having to change the configuration or the wiring. IM Module: https://support.industry.siemens.com/cs/de/en/view/26291781 If you don’t require the new functions, you can continue to work with older STEP7 versions. The new modules are spare part compatible with the modules shipped up to now. This means that you can retain your configuration when you replace a module. The new modules will also work with the existing (old) configuration. The new functions of the module are described on two Product Information bulletins that you will find under entry IDs26269772 and 26269778. Regards |
1/12/2016 11:00 AM | |
Joined: 8/9/2014 Last visit: 7/14/2023 Posts: 16 Rating:
|
Thanks for the prompt response. There is one more query. As there are 4 IM cards in use(Redundant System). If we replace one of them with their successor. Then Do we need to replace the rest 3 also with the successor or not. |
1/12/2016 11:52 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Rajat, As the manual says, the redundant devices have to be the same. SIMATIC S7-300/S7-400 Software redundancy for SIMATIC S7
hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
Follow us on