Industry Online Support
Technical Forum
5/30/2012 7:09 AM | |
Posts: 58 Rating: (19) |
Dear True_Blue, The following FAQ link might help you. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=13305690&treeLang=en Regards Ajay Gupta |
6/11/2012 6:12 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328) |
I posted a program to sync time between S7 and S120 in the german forum: /tf/WW/de/Posts/40519#top As I read your post,I quickly translated the "manual" (I hope it has not to much spelling errors) and my lastpost in the german forum: ------------------------------------------------------ I used STEP 7 and STARTER The S7-project is attached. I skipped the reading of the answer from the S120 (after it worked). So the writing commands are now sended blindly (Without checking the answer). It it worked, you can see in parameter 3102 or in STARTER (in the time stamp after generating a new error) . --------------------------------------------------------- Attachmenttimesync.zip (271 Downloads) |
Last edited by: miami at: 6/11/2012 6:14 PMLast edited by: miami at: 6/11/2012 6:12 PM |
|
Follow us on