10/9/2016 12:17 PM | |
Joined: 12/18/2014 Last visit: 12/6/2023 Posts: 31561 Rating:
|
This is because the LOGO! is in the operating mode. Then the menu is restricted and the function "start / stop" is dimmed. You must use the LOGO! to the ADMIN mode. You need the password. In the delivery state, the password is "LOGO" (without the quotation marks). See attachment. AttachmentLOGO! 8 Soft manual 0BA8 2014_06 sides 63+64 (OP-ADMIN).pdf (36 Downloads) |
This contribution was helpful to
1 thankful Users |
10/9/2016 12:23 PM | |
Joined: 9/12/2011 Last visit: 9/14/2023 Posts: 61 Rating:
|
Thank you so much |
George Awny |
|
This contribution was helpful to
1 thankful Users |
Follow us on