6/16/2016 5:39 AM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
Which Logo do you use? You have written so far only the software version, not the Logo-type (0BA8 or other)? |
6/16/2016 7:46 PM | |
Posts: 7 Rating:
|
It is a LOGO! 0BA8 If it is not possible, is there other hardware/software that will make such a thing possible? |
6/16/2016 8:06 PM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
You can change via display in a message text each weekday (on or off). Maybe for you is enough this. |
6/16/2016 8:16 PM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
Here a simply example.
AttachmentWeekly_timer.zip (87 Downloads) |
6/17/2016 8:12 AM | |
Posts: 2930 Rating:
|
Hi, here an example: In the example after DL to LOGO! press ESC >1 sec then you can change day, Ton and Toff of Cam1 from a weekly timer. Your question is a beginner question. I suggest you to use the LOGO! WBT to at least get the basics for LOGO!. You will get experiances with LOGO! and good new ideas to improve your application. Hope this helps AttachmentForum.zip (71 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on