7/9/2013 5:15 PM | |
Posts: 1547 Rating:
|
Hi, this is not possible with any TIA Portal function, but you can create an own application on PC using native TCP connection. The PC will establish the connection to the PLC and the PC will set the bit continuously. The PLC will reset this bit each 5 seconds. If the bit goes down the PC or the application can't reach the PLC. You can use following blocks to realize the function: How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300 or S7-400 CPU? |
This contribution was helpful to
1 thankful Users |
7/9/2013 9:47 PM | |
Posts: 7 Rating:
|
OK. I will give it a try. Thank you for the answer! |
1/11/2017 8:47 AM | |
Posts: 1 Rating:
|
Instructions->Extended instructions->Diagnostics->LED status |
Follow us on