9/16/2014 11:04 AM | |
Joined: 8/31/2005 Last visit: 3/13/2025 Posts: 2198 Rating:
|
Do you talk from a PC with the SoftPLC WinAC? It will help ust to help you, if you tell us which bus system (e.g. PROFIBUS or PROFINET) you have at the S7-PLC. And if you have STEP 7 V5.x or STEP 7 in TIA Portal (V11 or higher). Assuming you have If you use STEP 7 V5 (and not STEP 7 in TIA Portal) and PROFIBUS or PROFINET you may use this: http://support.automation.siemens.com/WW/view/en/98278878 In STEP 7 (any version) you can select "reachable notes/Accessible devices". This will list all stations on PROFIBUS or PROFINET that can be reached from the programming PC. If you use PROFINET you may use this: http://support.automation.siemens.com/WW/view/en/67460624and http://support.automation.siemens.com/WW/view/en/24000238 |
|
|
9/16/2014 1:58 PM | |
Posts: 4 Rating:
|
OK, it’s definitely Profibus. Screen shot attached. Main CPU is 9311.06 |
9/16/2014 2:08 PM | |
Posts: 4 Rating:
|
Here is a screen shot of the main panel for layout etc. As you can see, just a few alarms |
Follow us on