4/10/2014 12:52 PM | |
Joined: 9/19/2009 Last visit: 4/8/2025 Posts: 459 Rating:
|
Hi everybody Following this information, SIMATIC Logon can be installed on the HMI system itself or on another remote PC in the network or a domain controller. When SIMATIC Logon is used, the use of a chip card reader for user authentication is also supported. I understand that is possible use Simatic Logon, with Chipcard. I have tried this with WinCC RT Advanced but I can´t work with chipcard. by the way I have tried with WinCC RT Professional and no problem, works perfecty Simatic Logon works fine with WinCC RT Advanced, but the option of chipcard don´t work. Anyone has tried? Is possible to use it? |
Last edited by: JM76 at: 4/10/2014 12:52 PMIf my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/10/2014 4:35 PM | |
Joined: 9/19/2009 Last visit: 4/8/2025 Posts: 459 Rating:
|
Thank you very much for your tip I believe that, but I didn´t know sure. Thanks again |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on