Industry Online Support
Technical Forum
6/4/2012 1:32 PM | |
Posts: 35 Rating:
|
Dear DenisMor, Thank you for your answer, and I have one more question regarding Built in encoders (Resolver, absolute, incremental ... etc). If I'm using SINAMICS S120 and a motor with built in encoder with a DRIVE-CLIQ interface. Could you please explain briefly what are the factors that would affect my choice regarding the Encoder type? MEANING: Why would I choose an Incremental encoder in one case and an absolute in another case? and If the answer is : It depends on the application itself, then what are the factors in a certain application that would affect my selection. Thanks in Advace, M.G. |
6/4/2012 2:27 PM | |
Posts: 344 Rating:
|
Check out the Encoder Selection forum thread. It answers your question. |
6/4/2012 2:47 PM | |
Posts: 35 Rating:
|
Dear DenisMor, Really appreciate your answer. Regards, M.G. |
Follow us on