3/16/2012 8:10 AM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
Hello, The rules concerning Profibus are Minimum cable length for PROFIBUS-DP net work Acceptable line length in PROFIBUS-DP networks and What should you watch out for when using the RS485 repeater in PROFIBUS and MPI bus systems? Check also the manual which is mentioned in all three FAQs. About the type of cable: copper or FO (in case need 'convertor'). Copper type of cable - a lot manufacturers (Siemens, Belden, ABB...). Belden DataBus Cables For PROFIBUS Applications PROFIBUS cable Profibus Installation Guideline Best regards, Hristo Mihalev |
Follow us on