6/17/2010 1:10 PM | |
Joined: 10/7/2005 Last visit: 9/19/2024 Posts: 3021 Rating: (1054)
|
That is absolutely correct dear Miguel.
Spot on correctagain. As it turns out, there is (seriously old but still relevant) FAQ concerning this and you can find the link to it below:: Behavior of the communication processors during data transfer via TCP connections without RFC 1006 Last but not least, THISlink mentions that you can use TSEND and TRCV also in combination with a CP443 (-1EX40 or-1EX41). The compatibility pdf that is available in THIS newer link however does contradict the above information. One of them is obviously "wrong" (or out of date), but just in case you use a 1EX40 or1EX41 CP443 it may be worthwhile to verify this with a service & support request as it may solve you some programming effort. I hope this helps |
Cheers |
|
Follow us on