1/31/2018 10:45 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello ALCRZ; You have too many questions for my level of expertise, I couldn't give you all your answers. So let's see if Siemens documents can provide some informatiion. You will find in this list the Ethernet ports used by S7 CPUs and CPs to communicate, and suggestions for the Description of the CP 343-1 Lean - Industry Support Siemens In this manual for the CP 343-1 Lean (entry-level Ethernet communication processor for the S7-300 family) you will find some basic information on the use of HTTP, SNMP (as agent) and Telnet connections. See the screenshot below for more details. As per your question on password protection on a S7-300 CPU, the following FAQ can guide you: How can you activate the protection level with a password in the HW Config for an S7 CPU? Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 2/1/2018 12:12:50 PMInserted right links. |
|
This contribution was helpful to
1 thankful Users |
2/2/2018 2:16 AM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello AL; Somehow I believe the following documents can be of help. It seems password protection is not effective agaist Telnet or other intrusions, and cybersecurity measures are the only protection suggested by Siemens. I have found no document from Siemens showing the possibility of disabling Telnet and other accesses on their CPUs. Network security - SiemensExploiting Siemens Simatic S7 PLCs - Black HatIf we were to compare ISO-TSAP to the TELNET protocol or HTTP, we will find some commonalities. Everything is transmitted in plain text, for example. If an attacker were to record the traffic, they could easily extract data such as user names, passwords, commands, negotiated sessions, logic, etc. Any of these variables could lead to a full system compromise of the PLC. Attackers could also perform a man in the middle (MITM) attack against the engineering workstation while it is transmitting information to the PLC. Interestingly enough the Simatic PLCs under test, use each of these protocols, and services. The S7- 300 has a telnet server and web server running on it, and the S7-1200 supports both HTTP and HTTPS (the proprietary Siemens PLC web server is known as “SimaticHTTP.”) These have yielded some interesting results during my fuzzing session against the S7-300 and S7-1200. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/2/2018 4:03:52 AM |
|
This contribution was helpful to
2 thankful Users |
2/6/2018 5:08 PM | |
Posts: 3 Rating:
|
Hi Daniel, Thanks again a lot. I finally found what I needed, or most of it from this manual: https://support.industry.siemens.com/cs/ww/en/view/109745536 I truly appreciate the assistance. Thanks, AL |
Last edited by: Jen_Moderator at: 2/7/2018 1:34:47 PMOptimized link. |
|
This contribution was helpful to
1 thankful Users |
Follow us on