8/22/2014 6:32 AM | |
Posts: 5 Rating:
|
I am trying to use a clock bit to enable a GETblock at the REQ parameter. I have enabled the use of the clock memory byte and am using that tag. When I monitor the value at the tag it just reads false. I am new to S7 and I wonder if I have a basic setting wrong somewhere. Anybody got an idea what I could check? I have attached my program. Thanks! AttachmentProject30.zip (32 Downloads) |
8/22/2014 8:09 AM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
It's a TIA v13 project, perhaps you can make some printscreens as well for those who have not installed V 13 (yet). Check the notes Georgio wrote. Faq: How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to
2 thankful Users |
8/22/2014 8:23 AM | |
Posts: 5 Rating:
|
Thank you. That was what I was doing, I was overwriting them another place in my program. Thanks for the help! |
This contribution was helpful to
2 thankful Users |
8/22/2014 9:16 AM | |
Joined: 10/28/2008 Last visit: 10/29/2021 Posts: 243 Rating:
|
It's a TIA v13 project, perhaps you can make some printscreens as well for those who have not installed V 13 (yet). Check the notes Georgio wrote. Faq: How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? Regards, Marcjan I have TIA v13 installed, but I am unable to open the project Regards.
|
Georgio |
|
Follow us on