3/10/2016 11:36 AM | |
Posts: 2 Rating:
|
Hi, Denilson It's possible to close a pop-up screen with a TAG? i.e, when open the pop-up screen, it also sets a bit on the PLC and starts a timmer (Pext) and Set another bit(2). When this bit(2) is reseted - timmer finished, it closes automatic the pop-up window. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/11/2016 2:56:31 PMNew subject after splitting |
|
3/11/2016 12:45 PM | |
Posts: 2 Rating:
|
Thanks for your help. It's done :) |
11/21/2016 12:38 PM | |
Posts: 1 Rating:
|
Can I see the code example from the script? Cheers |
Follow us on