8/16/2018 4:40 AM | |
Joined: 2/28/2016 Last visit: 5/21/2024 Posts: 3 Rating:
|
Hi all, I have similar problem with Modbus RTU, so i decide ask for advise without create duplicate topics. Problem: I don't get "Done" from Master block. Once in first cycle it generate error "80CB". I check configuration on both sides (master and slave) and looks the same. If have someone advice where i should look or check, i I will be very thankful. Cfg hw: Master - CPU 1211C DC/DC/DC, 6ES7 211-1AE40-0XB0, V4.1 with CM 1241 (RS422/485), 6ES7 241-1CH32-0XB0, V2.1 Slave - Modbus Slave (from modbustools) Connection by RS485 (pin 3 - B , 8 - A and ground - 1 according to the datasheet) Attachment include photos of configuration and prj (if it's will be more useful for someone) ------------------------------------------------------------------------------------------ AttachmentS1200ModbusRTU_cfg.zip (54 Downloads) |
Last edited by: Jen_Moderator at: 8/16/2018 7:38:25 AMNew subject after splitting |
|
Follow us on