5/10/2017 6:58 PM | |
Posts: 34 Rating:
|
Hi everyone, I'm serching for CM101 gateway module electrical information (Input current, Power loss ..). Can someone help me. Thanks. |
5/10/2017 9:31 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello Amen; I can find very little information on this PCS 7 gateway CM 101 (Modbus RTU/Modbus TCP) except for this very slim document: Modbus Gateway CM101 PCS 7 driver blocks - Siemens Support All you learn there is that you have to provide the module wiuth 24 VDC (9-32 VDC to be exact). I have located no further technical data sheets for this module available on the web. I have found another flyer on a PCS 7 gateway for IEC 61850, the CM 104, also very poor on technical information. But it has a contact email that you might want to try at the back of the brochure,so you could request the technical data for your CM 101. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/10/2017 9:33:40 PM |
|
Follow us on