1/19/2016 11:21 AM | |
Joined: 8/31/2013 Last visit: 1/12/2023 Posts: 592 Rating:
|
HelloFredrik567 Firstly Like these Problems you should check your Cables sockets , Measurement the Signals should be about 10.8 to 12 V if you are using RS485 communications. Second Check the distance of your communication. Third Check your Boud rate and check if your distance is suitable to it. |
Warm Regards |
|
This contribution was helpful to
1 thankful Users |
1/20/2016 2:44 PM | |
Posts: 5225 Rating:
|
Look at the instruction that you use to set the baud rate. Consider all the time related parameters. w |
5/16/2016 6:40 PM | |
Joined: 8/8/2014 Last visit: 9/12/2022 Posts: 34 Rating:
|
My Master Block in attached file |
Follow us on