8/6/2019 9:44 AM | |
Joined: 4/24/2006 Last visit: 4/24/2025 Posts: 8965 Rating:
|
Hello, Here is a link to manual: Manual AS-i Master CM 1243-2 and AS-i Data Decoupling Unit DCM 1271 for SIMATIC S7-1200 See chapter 7.2 This LPF is True when AS-i slave signals I/O faults Best regards, Wizard |
8/6/2019 10:32 AM | |
Joined: 1/6/2009 Last visit: 4/21/2025 Posts: 137 Rating:
|
Hello, I understood this part, but my question it will seem stupid but what is an I/O fault? I know that can be a failure in an input or output, but what failure? a short circuit in an input? I test it and it remains false. Can be a output that was activated but the slave don't have the 24VDC for outputs? I tested it and the flag remains false. Regards, Nuno. |
Follow us on