2/7/2016 7:50 PM | |
Joined: 12/18/2014 Last visit: 1/16/2025 Posts: 34498 Rating: (4306) |
The outputs of the CMR are transistor outputs. You probably measure 24VDC with a digital meter with a very high internal resistance. Edit: Are the output control LEDs off? AttachmentSide 126.pdf (250 Downloads) |
Last edited by: ixo65 at: 2/7/2016 7:51:36 PM |
|
2/7/2016 8:34 PM | |
Joined: 9/7/2010 Last visit: 8/27/2024 Posts: 50 Rating: (2) |
Sorry about editing. ,
|
2/7/2016 9:05 PM | |
Joined: 9/7/2010 Last visit: 8/27/2024 Posts: 50 Rating: (2) |
nothing was wired to the outputs until now and it is an - led 2 mA |
Follow us on