6/23/2015 11:02 PM | |
Joined: 8/16/2014 Last visit: 7/25/2024 Posts: 10 Rating:
|
Hello, I have a new code reader Datalogic Matrix 300N™ (Profinet-IO communication embedded) and I unsuccessfully trying to connect to this device in TIA Portal V13 SP1. 1) First I downloaded GSDML file and I installed it. 2) I added my device Matrix 300N from HW catalog to HW configuration. In network view I connected this device to CPU. I have set a IP address and profinet name. All I dowload to PLC. After download, PLC goes to STOP witch errors (blinking red)... I see my device in Distributed I/O same as et 200sp or CU320 units, my reader device is "not reachable". In Online&Diagnostics i can't see nothing. No MAC address, no chance to change name or IP adress ... "not reachable" Could anybody to help me, please? |
6/25/2015 7:27 AM | |
Joined: 5/15/2012 Last visit: 5/21/2024 Posts: 39 Rating:
|
Hello,
I think Standalone mode is OK.
What IP address and mask have PLC and what IP and mask have Reader? (Manual say default is 192.168.3.100.) Can you ping Reader from PC?
Look for manual: Matrix 300N Reference Manual.pdf (manufacturer webpage), page 8(paper) / 20(reader) -> Device Discovery page 79(paper) / 91(reader) -> 4.7 ON-BOARD ETHERNET INTERFACE http://www.datalogic.com/eng/products/industrial-automation/fixed-industrial-barcode-readers/matrix-300n-pd-659.html (Downloads / Manuals) Palo |
Last edited by: Palo PLC at: 6/25/2015 7:36:49 AMLast edited by: Palo PLC at: 6/25/2015 7:38:17 AM |
|
This contribution was helpful to
1 thankful Users |
5/26/2021 1:35 PM | |
Joined: 12/26/2015 Last visit: 8/17/2024 Posts: 2 Rating:
|
Fyi
AttachmentHow to run a Matrix N over PROFINET-IO_TIA.pdf (1206 Downloads) |
This contribution was helpful to
1 thankful Users |
5/26/2021 1:36 PM | |
Joined: 12/26/2015 Last visit: 8/17/2024 Posts: 2 Rating:
|
AttachmentHow to run a Matrix N over PROFINET-IO_Simatic.pdf (854 Downloads) |
Follow us on