6/3/2011 8:04 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi Here is link http://support.automation.siemens.com/WW/view/en/18797552 manual page 208 " These GSD files are located in the "WinCC flexible Support\PlcProg\GSD" directory. Different GSD files must be used depending on the particular HMI device:" |
Last edited by: Heksu at: 6/3/2011 8:08 AM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
6/3/2011 8:17 AM | |
Joined: 8/25/2006 Last visit: 10/9/2024 Posts: 2209 Rating: (279) |
You may download this gsd-file here: find in table SIMATIC S5 *). |
6/7/2011 6:36 AM | |
Joined: 10/7/2005 Last visit: 10/9/2024 Posts: 3024 Rating: (1054)
|
Step 1: Copythe GSD file into the "GSD" directory of your COM Profibusinstallation directory Step 2:Use the"Read in GSD files" command from the COM Profibus"File" menu The aboveas well as more very helpful information is available in the COM Profibus manual and I hope it helps. |
Cheers |
|
6/13/2011 4:32 AM | |
Posts: 71 Rating: (0) |
Hi All, Thanks for your help. However im now missing another gsd file SEW_3100.gsd. Where can i download this file? Thanks |
Follow us on