Industry Online Support
Technical Forum
2/26/2009 10:10 AM | |
Posts: 6 Rating:
|
Hi friends! Thank u very much, INS. I have replaced the cable with a new one and everything seems to be better. I stillutilise a crossover cable ( pin1-pin3, pin3-pin1, pin2-pin6,pin6-pin2) to link my PC to the CPU. This time, the symptoms are: Link Leds turn 'ON' and PC reports: 'connected'. However, this only lasts for approx. 10 seconds and then: Link Leds turn' OFF' along with the announcement 'cable unplugged' on my PC. Everything,subsequently, happens as in a dance floor: 'ON' about 10 sec, 'OFF' about 3 sec...Ithere cannot download my HW configuration to the CPU via PROFINET. Is there still anything wrong? Must I download my HW configuration to CPU via MPI connection first(communication via MPI connection is always OK)? I attach my simple project. Pleasetake a look and help me to find the reason. Thanks for your helpful supports! Best Regards, Hoang Viet. Attachmentthu_conf1.zip (265 Downloads) |
2/27/2009 9:12 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi, I think there is something wrong with your firewall or with the installed protocols on your PC. There is also an FAQ about this on the Support site. Why do no PROFINET components appear in the primary setup tool or in STEP 7 -Display Accessible Nodes-? I hope this works. |
Best regards, |
|
Follow us on