6/29/2018 2:53 PM | |
Joined: 3/11/2014 Last visit: 10/28/2022 Posts: 5 Rating:
|
Hi all, I am trying to communicate a remote ET200SP with a PM210 multimeter of the SCHNEIDER brand, through MODBUS RTU (RS485). However, my MODBUS_MASTER block does not receive slave data on the DATA_PTR, but the RX / TX LEDs are flashing during the request. In the multi-meter I only have the option of setting baud rate, MB Adress and parity, these are configured according to the block. The BUSY output stays in DONE during the request, but the DONE output never changes stains. Did they have any suggestions? Brazil's support could not identify anything wrong. AttachmentCM PTP - PM210.zip (141 Downloads) |
Follow us on