8/7/2013 8:01 AM | |
Joined: 7/4/2013 Last visit: 4/6/2023 Posts: 1 Rating:
|
In S7300 plc,while downloading program to plc.comments will be stored in Load memory or it remains in PG/PC. |
8/7/2013 8:02 AM | |
Posts: 1064 Rating:
|
comments are not loaded they stay in the pg |
8/9/2013 3:40 PM | |
Joined: 9/27/2006 Last visit: 10/2/2023 Posts: 12153 Rating:
|
Hello Piotr; Your rant is misinformed and undeserved. As Pranav mentionned earlier, whatever space available on the memory card once the PLCprogram is loaded can be used to write files, archives and even drawings for your project. this functionnality has been available since the early days of Step 7 5.x, this FAQ for example dates back to 2007: How can you load projects to a memory card and back again to a PG/PC? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/9/2013 3:40 PM |
|
This contribution was helpful to
4 thankful Users |
Follow us on