2/29/2016 12:02 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Steve, This manual will help: CPU-CPU Communication with SIMATIC Controllershave a look on page 95 to see what kind of ethernet-communication is possible. For PUT/GET with CPU317 and CP341-1lean as server you must activate the PUT/GET-access in the proberties of the DB that should be accessed. For Open Communication there are several FAQ´s: How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?This FAQ also exists for UDP and ISO-on-TCP protocol. hope this helps, regards, |
FCK WAR! |
|
Follow us on