5/1/2012 7:53 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello Piku, For Master Master Communication(profibus), you need to use DP-DPCoupler. herei found link to download the manual DP/DP Couplerfor your reference. Hope this will give some idea. Also, you will get so many thread if you just search in with DP-DP Coupler. |
VANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
5/1/2012 10:35 AM | |
Posts: 947 Rating:
|
may be should other plc make slave and coomunicate with master "master-slave"& |
5/1/2012 4:06 PM | |
Posts: 559 Rating:
|
Dear Piku, On which CPU u r working? Do u have Free MPI Port available? Then u can for the GD Packets communication. Please find the attached manual for the same to configure it. Attachmentcp_e12_0_2_e.pdf (127 Downloads) |
This contribution was helpful to
3 thankful Users |
5/1/2012 4:15 PM | |
Posts: 59 Rating:
|
Thanks SolutionFinder, It is very good idea for communication. I also knew this first time. |
5/2/2012 7:39 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
hi amit, i think this is only for same brand (siemens).may not work for two Different brand of master PLC Communication, regards, viral |
5/2/2012 8:21 AM | |
Posts: 13 Rating:
|
Dear Solution finder , Im working on S7-300 Cpu (315) and i hav two DP ports available. will it work as per youyr suggestion for the cpu? |
Follow us on