3/28/2016 11:01 AM | |
Posts: 7 Rating:
|
Thanks for your answer. I want to create an application with C# in PC, to receive the inputs status of PLC (S7 300). I connect the cp 343-1 module to a modem via a LAN cable. also I connect my PC to modem via wifi . I have not any error in module in hardware, and the SF LED in module is off. But in my project in TIA Portal the module has an error . error : "OK, Error in lower-level component" and I find that error is : "no valid configuration data found." please see the screen shoot in attachment. Also I used AG-Send, AG-CNTEX, AG-UNLOCK, for communication. But i faced to another problem and I can not find the device ID, I faced error 8186 in status of this blocks, that shows the ID input is not valid. Please check the screen shoot (8186 error) in attachment . If you have any idea, please help me. Thanks a lot. AttachmentScreenshots.zip (216 Downloads) |
Last edited by: hiva_company at: 3/28/2016 11:06:51 AM |
|
10/4/2017 8:35 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by sonarao is split to a separate thread with the subject CP 343 show SF fault . Best regards |
Follow us on