Industry Online Support
Technical Forum
12/11/2014 6:27 AM | |
Posts: 5225 Rating: (1197) |
Hi. The company that put their badge on this product might be helpful to you. I suggest you ask them for some information on how to link via Profinet. You might be lucky enough to get a sample program. Try [LINK]. If you could return with a sample program the Experts will be of much more help. Also.. For communications between drive and PLC a block memory is allocated. The data that flows out of the device is buffered through "outputs" and data flowing into the device is buffered through "inputs". This is a bit confusing as the inputs and outputs is not physically going outside.. it is in this case "virtual". But the program handle these as if they are real physical inputs and outputs. The term "telegram" is used to describe how the data is packaged. For example the first WORD in the package might indicate SPEED.. but it could easily have been a group of boolean commands. Only the supplier can tell you how the data is packaged so that you can write the program to translate the data into information. I ask you to do some footwork at the manufacturer for information that will be helpful to the Experts to assist you further You can also have a browse though the forum pages for descriptions on what the difference is between FC / FB / DB and so on - even better if you can find a Siemens rep. to give you a quick tour to what PLCs are about. PLCs are different than what you are know, but I have confidence that if you can do C, you can get a PLC up and running in a short time. Greetings. |
Follow us on