6/21/2016 6:49 AM | |
Posts: 37 Rating:
|
Dear Experts, I want to establish communication and setup data exchange between s7-400 & s7-300 station. The network is established which is TCP/IP over wireless. station are pinging each other. what are best blocks for communication. Can I use AG_SEND & AG_RECV on both sides. Please suggest Regards, Udaybhaskar ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/21/2016 9:14:24 AMNew subject after splitting |
|
6/21/2016 8:32 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Desi boyz, I recommend you to have a look in this amazing manual: CPU-CPU Communication with SIMATIC Controllers page 96 will show you all posibilities for communication between S7-300 and S7-400. You can even see, which blocks to use. hope this helps, regards,
|
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
Follow us on