5/26/2009 9:18 AM | |
Posts: 3 Rating:
|
This is a dcs system .IA & B are remote I/O's acting as slave to main Dcs.The Distance bet A & B is 200m & Distance between Main Dcs & this two slaves is approx.1 km.All communication based on ethernet .converter is used to convert ethernet to optical fiber link & vice versa,for both I/O's. Also plz suggest if any extra requirements /module require to establish comm.. Attachmentcommunication Bet two slave with dcs.zip (29 Downloads) |
Follow us on