11/15/2013 8:00 AM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
|
This contribution was helpful to
2 thankful Users |
11/15/2013 8:17 AM | |
Joined: 4/25/2011 Last visit: 1/19/2025 Posts: 128 Rating:
|
Dear Sir, I have created program in netpro, and also copy the programming blocks from example , earlier i got from this portal. But still communication not established and showing ERROE bit 1 and STATUS bit also 1. I am attaching my project here . Please check it..... Thanks & Regard's Attachment314-2PN_DP.zip (175 Downloads) |
Naveen Paliwal |
|
11/15/2013 8:19 AM | |
Joined: 10/7/2005 Last visit: 3/18/2025 Posts: 3042 Rating:
|
Hello naveen_paliwal there are several ways to skin this cat and I can't tell which one is "the best" as it depends on your application (e.g. how much data, how fast etc.). Arguably the easiest way is via an S7 connection and usageof GET/PUT and you'll find an example for it at How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU? Note that you need to grab the FB14/15 GET/PUT Blocks from different folders for each of your PLC's as mentioned in the above link and also shown below:
|
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on