2/20/2014 9:10 AM | |
Joined: 10/7/2005 Last visit: 4/17/2025 Posts: 3047 Rating:
|
Hello SAMIRKM further to the advise that was given, have a look at chapter 14.5.1 of the SIMATIC Fault-tolerant systems S7-400H manual and note the entry about GET/PUT at the end which states that: (Use) SFB 15 "PUT" and SFB 14 "GET" in the fault-tolerant system: Use two SFB 15 "PUT" blocks over two standard connections. successful. If possible, use the mechanisms of S7 communication for communication. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on