4/13/2022 11:53 AM | |
Joined: 3/14/2022 Last visit: 8/26/2023 Posts: 3 Rating: (0) |
Hello everyone finally I found a pdf that was useful but I have some problem with create certification on CF cart and I didn't understand paragraph below on page 5 of the PDF that I attached.
to enter the Simotion compact flash folder with username and password, type the following path: FTP: \\ admin: pluto@192.168.0.77: where admin is the username bar is the password 192.168.0.77 is the IP address of the connection port while the certificates to be replaced are located in the following path: ftp://192.168.0.77/USER/SIMOTION/HMICFG/certstore/OPCUACerts/
AttachmentOPC UA for Simotion.pdf (630 Downloads) |