Industry Online Support
Technical Forum
3/29/2010 3:53 PM | |
Joined: 12/9/2009 Last visit: 4/5/2022 Posts: 156 Rating:
|
Hello, it`s possible to exchange data between S7-200 and S7-400H system via Industrial Ethernet. You can use S7 communication. You will need two connections. One connection to each CP443-1. Under the following link you can find an instruction for configuration: http://support.automation.siemens.com/WW/view/en/17369594 The S7-200 is configured with STEP 7 MicroWIN. Best Regards Little Holmes |
This contribution was helpful to
1 thankful Users |
Follow us on