4/7/2009 10:38 PM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User
|
9/23/2009 9:19 AM | |
Joined: 8/20/2009 Last visit: 11/6/2024 Posts: 80 Rating:
|
I was facing similar problem with Masibus Temperature scanner, also. What I found is that the temperature scannercommunicateson modbus on Station address = any unique, Baud rate = 9.8 kbps/19.2 kbps, Stop bit = 1 andParity= none. So, you should have this settings in the parameter configuration of modbus master. The rest is the communication programming. For that you can use project library on modbus. Or go through the program attached. Regards, Vishal Parmar. Attachment8106__36_220609.zip (534 Downloads) |
Vishme. |
|
This contribution was helpful to
1 thankful Users |
Follow us on