3/26/2008 1:06 PM | |
Posts: 5822 Rating:
|
Hello, I have to admit, I am not that deep into flexible, but I hope I can help at least about the routing issue. J_Bell |
3/26/2008 1:59 PM | |
Posts: 6 Rating:
|
[quote user="J_Bell"]Have you already read the FAQ: How do you use WinCC flexible 2005 to transfer a project to an operator panel via S7 routing? Yes, I have already read that FAQ and the entries it links to and my system is set up according to all the instructions given there. Maybe I can provide some additional information to diagnose the problem? If so, feel free to ask. Best regards, Marcin Goliszewski. |
Follow us on