11/11/2010 12:44 PM | |
Posts: 13 Rating:
|
Dear chartier, I have one F-cpu (315F-2DP) and one H-Syatem (414-4H). Now I have to send the 240 bytes data from F-CPUto H system and Recieve 850 bytes from H system to F -CPU. Communication is on, from CPU315-2DP we used CP343-1 lean module and for H-System, we used CP 443-1 module. I am done this using FC5 and FC6 (AG-SEND and AG-RCV block) on both side F-cpu and H-Syatem. will it be worked or not? Splitted from Distributed fail safe syatem . |
Last edited by: O_Moderator at: 11/11/2010 2:57 PMnew subject after splitting |
|
11/11/2010 2:59 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread Data Send and RCV between F-CPU and H-CPU. Best regards O_Moderator |
Follow us on