3/18/2013 9:08 PM | |
Joined: 6/23/2008 Last visit: 2/9/2025 Posts: 1168 Rating:
|
Hello, CP or no CP should not be the question (for at first). PLC or no PLC is the question... If you would have given an answer to Kampi's question regarding the order nr we would know if you are maybe talking about an ET200S with integrated CPU. But, by what I read in your thread I have the feeling that you would like to connect a simple ET200S (without a CPU) to your PC and you would like just access the In/Outputsfrom your application. I think this is not so easily possible... A more easily way could be that you run a "Soft-PLC" on the PC. This could be the logical controller coming with the product "WinAC" from Siemens. This controllercan beprogramed with Step7. Also HW-config for this controller including the ET200S can be done with Step7. It could be done on a separat PC with Step7 and then downloaded to the PC with the logical controller. You need to create a minimum S7 program in wich some memory (for example DBs) is written to outputs and where the results from the inputs isstored. In addition you could run an OPC-Server on this PC. With this OPC-Server you can relativ easily acces this memory too. Your application wich is created with visual studio could than communicate with the OPC-Server. There should be some documention in the www how an application can access data from an OPC-Server because this is what OPC was invented for. If you need a CP or if you can use a network card for the profinet IOis a question of supportby the locical controller. Which "normal" network cards (and also which CPs) can be used with "WinAC" you can find in this documentation on page 125: Link Regards... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
3/19/2013 9:18 AM | |
Posts: 30 Rating:
|
thankx...atleast now i get the idea that how this work is possible... right now i also have the CPU 317F-2PN/DP (S7-300).. i also have the Step 7 Software... this plc also have the DI 32 module and also same DO 32 Module.... so please give me any kind of manual where i can start work on this PLC.. if i get the successful result after that i will buy the "WinAC"... First goal on this PLC is to attach the MV420 Siemens Camera.. after that get the response from this camera using OPC... so please first give me the hardware Config ...
|
3/19/2013 9:45 AM | |
Posts: 366 Rating:
|
Maybe at first the manual in the attachment will help you! nice regards AttachmentS7P.pdf (620 Downloads) |
8/8/2014 12:01 PM | |
Joined: 9/1/2005 Last visit: 3/10/2025 Posts: 4113 Rating:
|
new question published by kartikkaptais split to a seperate thread with the subject How can i get data to MS-Access database? Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on