12/7/2010 3:07 PM | |
Joined: 9/27/2006 Last visit: 3/14/2025 Posts: 12344 Rating:
|
Hello marcopolo; In the following link you will find a sample applicaytion to use a IM 308C as a DP-,master station(note the model of the IM card, this will not work with a IM 308B for example) with a CP 315-2DP slave. How do you operate an S7-300/400 as a DP slave on the PROFIBUS DP when the DP master is an S5 (with IM 308-C)? You will alsoneed the gsd file for the CPU 314-2DP that you plan to use in your application. You will find it here: PROFIBUS GSD files : SIMATIC Using the 2 links, you should be able tomodify the original programs and implement you own project. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/7/2010 3:09 PM |
|
This contribution was helpful to
2 thankful Users |
12/14/2010 7:51 AM | |
Joined: 10/7/2005 Last visit: 3/14/2025 Posts: 3042 Rating:
|
Hello Marcopolo I understand that you have a bunch of S5's, a Ethernet H1 network between (some of?) them,a Profibus L2 network between (some of?) them (FDL commsor Profibus DP?), one or moreHMI's (connected to what Network1?) and are about to add a Profibus DP Network via an IM308C to one of the S5's. My understanding may be totally wrong though, but either way,I must admit that I don't quite understand what you actuallywant to (or need to) do/achieve. Could you perhaps make a sketch or two and upload the here which show: 1.) The existing Network(s) 2.) The planned new additional Network. 3.) What comms need to go from where to where. The more detail you can give us (e.g type of comms cards), the better and I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on