12/10/2014 6:17 PM | |
Posts: 1 Rating:
|
has any one set up a TCP communication between s7 1500 and an old TI 505 PLC |
12/10/2014 7:40 PM | |
Posts: 510 Rating:
|
MI_Force, I have attached the CP-1434 TCP module manual. The manual contains a program example for communicating between a 505 and an S7 using an S7 CP card. It was written before the S7 CPUs had Profinet on the CPU. This should give you a starting point for your application. Unfortunately I do not have a working CP-1434 card for testing Good Luck, billwest AttachmentF:\pdf\PLC\505\505 CP1434-TCP.pdf (133 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on