Industry Online Support
Technical Forum
5/18/2010 9:58 AM | |
Joined: 8/7/2008 Last visit: 1/8/2025 Posts: 11 Rating: (0) |
Hello How to create, read and write a. Txt file on the hard drive of a PC via ethernet. S7-300 with CP343-1ex21 thanks |
5/19/2010 8:52 AM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, You can use for example the ftp protocol to read txt-files from the PC. To use the ftp protocol you will need a CP343-1 Advanced (for example CP343-1GX30). In the following manual you can find mor information about file ,anagement and file access with FTP: http://support.automation.siemens.com/WW/view/de/26701104 In the following manual you will find more information about the function blocks for FTP: http://support.automation.siemens.com/WW/view/en/30564821 Best regards Little Holmes |
Follow us on